Search
Languages

Bourns Introduces Metal Alloy-based, Multilayer Power Inductors Offering High Current Capability

The advanced monolithic construction of the CVH160808H Series supports higher current applications in a low profile, high reliability form factor

RIVERSIDE, Calif., October 29, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its CVH160808H Series Multilayer Power Chip Inductors. These new chip inductors are built with advanced multilayer technology to achieve a low profile, superior current capability solution that supports the higher current and space-constrained requirements of today’s consumer and communications applications.

The CVH160808H Series features a metal alloy-based core and monolithic construction offering high reliability, low DC resistance and high current capability in a compact form factor with a maximum profile of 0.8 mm. The new series has a rated current range of 1300 – 4000 mA, a DC resistance of 0.02 – 0.237 ohms and an operating temperature range of -40 to 125 °C. These features make Bourns® new Power Chip Inductors excellent power conversion solutions for mobile devices, wearables, tablets, laptops and various communication devices.

The CVH160808H Series Multilayer Power Chip Inductors are available now and are RoHS* compliant and halogen free**. For additional product information, please see: bourns.com/products/magnetic-products/chip-inductors-multilayer.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com