Search
Languages

Bourns Introduces Shielded Power Inductor Model Featuring High Heating/Saturation Current and Low Magnetic Field Radiation

Bourns’ advanced power inductor design provides performance, efficiency and safety benefits particularly suited to point-of-load converters and data center environments

RIVERSIDE, Calif., July 28, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its Model SRP1024HMCT Shielded Power Inductor. This shielded power inductor is manufactured using a hot press molding process with carbonyl powder and offers high heating current, high saturation current and low magnetic field radiation.

This new model is available in a space-saving low profile package, features low buzz noise and supports an operating temperature range from -40 °C to +125 °C. The advanced design and features offered with the Model SRP1024HMCT provide performance, efficiency and safety benefits making it ideal for point-of-load (PoL) converters and data center environments.

Bourns® Model SRP1024HMCT Shielded Power Inductor is available now through Bourns’ authorized distribution partners, and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com