Search
Languages

Expanding its Portfolio of Inductive Options, Bourns Releases High Current Rated AEC-Q200 Compliant, Automotive-Grade Shielded Power Inductor Series

Designed with ferrite core and ferrite shield for low magnetic field radiation, new inductor series is ideal for applications where low noise operation is essential

RIVERSIDE, Calif., February 10, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its new Model SRR6838A Series Shielded Power Inductors. Bourns’ new AEC-Q200 compliant, automotive-grade power inductors give designers of high reliability consumer, industrial and telecom applications an expanded range of inductive options.

Designed with a ferrite core and ferrite shield that delivers low magnetic field radiation, the advanced features of Bourns’ new power inductors make them a superior power conversion solution for applications that need to operate in low noise environments such as in automotive driver assistant, infotainment, and lighting systems. In addition, the Model SRR6838A Series provides excellent inductance and heating current capabilities featuring an inductance range up to 100 μH and heating current up to 6.8 A. These shielded inductors also offer a broad operating temperature range of -55 °C to +150 °C.

Bourns® Model SRR6838A Shielded Power Inductor Series is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com