Search
Languages

Bourns Releases High Precision Power Resistor Series Designed for High-Energy Pulse Applications

The Riedon™ BRF Series by Bourns features exceptional power ratings and TCRs delivering excellent energy dissipation for precision circuits

RIVERSIDE, Calif., November 24, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today launched its Riedon™ BRF Series Precision Power Foil Resistors by Bourns. Designed for high-energy pulse applications, BRF Series resistors feature exceptional power ratings up to 2500 W and a temperature coefficient of resistance (TCR) as low as ±15 ppm/°C. These features make them excellent energy dissipation solutions for circuits requiring high precision. In addition, this series is available in 2- and 4-terminal options with termination current ratings up to 150 A, giving developers the flexibility to tailor these resistors to their exact design requirements.

The BRF Series is built using metal foil technology housed in an aluminum heatsink and a low-profile package. Bourns specifically constructed its latest precision power resistors to meet the rugged and space-constrained requirements of a growing list of high-energy pulse applications such as power converters, Battery Energy Storage Systems (BESS), industrial power supplies, inverters, and motor drives. By combining outstanding power capacity with precision temperature stability, the BRF Series provides a versatile solution that supports the growing need for efficient, reliable, and accurate energy dissipation in next-generation high-performance systems.

The Riedon™ Model BRF Series High Precision Power Resistors by Bourns are available now and are RoHS* compliant. For additional information, please see: bourns.com/products/resistors/metal-foil-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com