Search
Languages

Offering ESD Protection Flexibility, Bourns Unveils TVS Diode Series Available in Space-Saving DO-214AB Package

New series with 21 unidirectional and bi-directional models features broad working peak reverse voltage range from 12 V to 30 V

RIVERSIDE, Calif., November 19, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today unveiled its 5.0SMDJ Series Transient Voltage Suppressor (TVS) Diodes. Available in a space-saving, compact DO-214AB package, the new series is designed to provide effective Electrostatic Discharge (ESD) protection for portable communications, computing and video equipment applications. The Bourns® 5.0SMDJ Series includes 13 unidirectional models and eight bi-directional models.

Offering high performance energy absorption and clamping capabilities, these new TVS diodes enable designers to select from a broad working peak reverse voltage range from 12 V to 30 V. The 5.0SMDJ Series also features peak pulse power of 5,000 watts and breakdown voltage up to 36.8 V with typical fast response times of less than 1 nanosecond to clamping after breakdown initiation. The series has also been tested to JEDEC standards.

The Bourns® 5.0SMDJ Series TVS Diode is available now through Bourns’ authorized distribution partners and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/diodes/tvs-diodes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com