Search
Languages

Bourns Announces Compact Common Mode Choke Series with Extended Current Capability up to 15 A and Broad Impedance Range

New automotive grade, AEC-Q200 compliant high current chokes have sector-wound configuration for enhanced dielectric strength between windings

RIVERSIDE, Calif., September 23, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its SRF7038A Series AEC-Q200 compliant, automotive grade common mode chokes. The new high current chokes feature an extended current capability up to 15 A and a broad impedance range of 70 to 3000 ohms. These features make the SRF7038A an excellent power line Electromagnetic Interference (EMI) suppression solution for use in consumer, industrial and automotive systems.

Furthermore, the SRF7038A Series helps resist electrical breakdown due to high voltage stress with its sector-wound configuration that enhances dielectric strength between windings. Plus, the series’ ferrite core construction with a closed loop magnet path provides greater magnetic shielding for low radiation that supports improved noise suppression. These high current chokes also have an operating temperature range from -40 °C to +125 °C.

The Bourns® SRF7038A Series automotive grade, AEC-Q200 compliant common mode chokes are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/common-mode-chokes-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com