Search
Languages

Bourns Adds New Common Mode Chip Inductor Series to its Growing Line of AEC-Q200 Compliant, Automotive Grade Magnetics Products

Ideal solutions for EMI suppression and noise filtering, these new inductors feature a compact size, deliver high impedance and support high current

RIVERSIDE, Calif., September 22, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today added a new common mode chip inductor series to its AEC-Q200 compliant, automotive grade Magnetics product line. Designed to provide effective EMI suppression and noise filtering, Bourns® SRF3225TAP Series Common Mode Chip Inductors feature a compact footprint, and deliver high impedance with values from 500 to 1000 ohms and support high current up to 2 A.

In addition, Bourns® SRF3225TAP Series has a shielded construction for low radiation while offering a broad operating temperature range from -55 °C to +150 °C. These features and capabilities make Bourns® latest inductors a superior choice for protecting sensitive devices, enhancing signal integrity and increasing reliability in noise filters and DC power lines in consumer, industrial, and other electronic products as well as automotive systems.

The Bourns® SRF3225TAP Series Common Mode Chip Inductors are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/common-mode-chip-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com