Search
Languages

Bourns Announces New Micro Encoders Offering High Reliability in a Compact Design

The PEC04 and PEC05 Series along with Model PEC06 all feature an IP40 rating offering a rugged, space-saving position sensing solution for a wide range of electronic devices

RIVERSIDE, Calif., August 4, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its PEC04 Series 4 mm Incremental Micro Encoder, its PEC05 Series 5 mm Incremental Micro Encoder and its Model PEC06, a 6 mm Incremental Micro Encoder. Bourns® new micro encoders provide position and speed information essential for control functions in a broad variety of electronic applications.

The Bourns® PEC04 Series is designed for use in today’s more compact consumer electronics such as micro headphones and smart wearable devices, and the Bourns® PEC05 Series is an optimal incremental encoder for mouse wheels, smart home appliances and smart wearable devices. In addition, the Bourns® Model PEC06 micro encoder is an ideal solution for smart home appliances and desk lamps, enabling designers to elevate the reliability of these next-generation intelligent devices.

The new micro encoders have an impressive IP40 rating for dust, feature a 30k, 50k and 20k rotational cycle rating respectively and a -20 °C to +70 °C operating temperature range in a rugged, compact surface mount design. These micro encoders also offer a 2-bit quadrature code output and 360-degree continuous mechanical angle. These features and capabilities make these micro encoders well-suited for space-constrained consumer electronics designs.

The Bourns® PEC04 and PEC05 Series as well as the Model PEC06 Incremental Micro Encoders are available now through Bourns’ authorized distribution partners, and are RoHS* compliant. For more detailed product information, please see: bourns.com/products/encoders/contacting-encoders.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com