Search
Languages

Bourns Announces Common Mode Inductor Series Ideal for Noise Suppression in Signal Transmission Line Applications

New inductors feature a low profile, compact size and provide high impedance over a high-frequency range

RIVERSIDE, Calif., June 4, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new common mode inductor series designed for noise suppression in signal transmission line applications. Bourns® SRF1209U4 Series Common Mode Chip Inductors feature a low profile, compact footprint that meets space-constrained design specifications. The new inductors also provide high impedance over a high-frequency range offering an enhanced signal to noise ratio, making them ideal for signal transmission line applications.

Bourns® SRF1209U4 Series is compatible with USB 3.1 Gen 1/2, HDMI 2.0/2.1, USB 4.0, and Thunderbolt interfaces. These chip inductors have an operating temperature range of -40 to +125 °C, impedance up to 90 ohms, current ratings up to 400 mA and a DCR of 0.3 ohms.

The Bourns® SRF1209U4 Series Common Mode Chip Inductors are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/chip-inductors-common-mode.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com