MENU
Search
Languages

Bourns Expands Shielded Power Inductor Portfolio with New Dual-Winding Series

Bourns® Model SRF3015 Series offers a cost-effective, space saving solution in a low 1.4 mm profile design

RIVERSIDE, Calif., October 28, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new cost-effective, space saving dual-winding shielded power inductor series. Bourns® Model SRF3015 Series features a low profile of 1.4 mm and shielded construction that provides low radiation making these inductors optimal solutions for attenuating high frequency noise in a broad range of circuits.

Bourns® latest power inductors offer an extended operating temperature range of -40 °C to +125 °C, and are particularly well-suited for use in SEPIC (Single-Ended Primary Inductance Converter) topologies and power supplies.

The Bourns® Model SRF3015 Series dual-winding shielded power inductors are available now, and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-dual-winding-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com
a