Search
Languages

Bourns Announces Two Automotive Grade Semi-shielded Power Inductor Series Engineered for High Reliability

Featuring bottom-soldered lead wire construction, the new series provides enhanced mechanical strength and stability making them ideal for mission-critical applications

RIVERSIDE, Calif., June 28, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced two new AEC-Q200 compliant, automotive grade semi-shielded power inductor series whose bottom-soldered lead wire construction offers enhanced mechanical strength and stability. Bourns designed the new Model SRN4012BTA and SRN4018BTA series as a high-reliability solution for mission-critical applications such as automotive systems, power supplies, DC-DC converters, and in various industrial and telecom electronics.

The Bourns semi-shielded structure combines the features of non-shielded and shielded inductors, providing lower magnetic field radiation than non-shielded inductors and a more cost-effective alternative to fully shielded ferrite-based inductors. These new ferrite core, enameled copper wire power inductors offer inductance values from 0.47 to 100 µH and an operating temperature range of –55 °C to +125 °C.

Bourns® Model SRN4012BTA and SRN4018BTA semi-shielded power inductor series are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com