Search
Languages

Bourns Introduces Low-Profile SMD High Current Shielded Power Inductors for DC/DC Converters in Mobile Electronics

Riverside, Calif., July 22, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced two new low-profile, small footprint SMD power inductors designed for DC/DC converters in mobile electronics applications. The new power inductor models, designated SRP2010 and SRP2512, feature inductance values from 0.22 – 2.2 μH with Irms up to 4.5 A and Isat (saturation current) up to 6.5 A. The dimensions of Bourns® Model SRP2010 is 2.0 x 1.6 x 1.0 millimeters (mm) and Model SRP2512 measures 2.5 x 2.0 x 1.2 mm making them ideal for a broad range of ultra-thin electronic applications including smartphones, tablets and data storage devices.

"Designers of today's multifunction mobile electronics applications continually demand smaller and thinner DC/DC converter solutions that must also meet their high current requirements. Bourns' new low-profile power inductor devices have been designed to satisfy these needs,” said Guido Zehnder, product manager at Bourns, Inc. "As excellent additions to Bourns' extensive line of power inductors, the latest devices offer the advantages of wirewound construction, and are designed with an iron powder core that features high saturation current and shielded construction for low magnetic radiation” said Zehnder.

Pricing and Availability As a pricing reference, the Bourns® model SRP2010 is priced at $ 0.22 each in 5,000 piece quantities. Both Bourns low-profile SMD high current shielded power inductors are available now and are RoHS compliant*. For additional product specifications, please go to: www.bourns.com/docs/product-datasheets/SRP2010.pdf and www.bourns.com/docs/product-datasheets/SRP2512.pdf.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011. Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com