Search
Languages

Bourns® High-Voltage, High-Energy GDT Series Offers Industry-Leading Surge Protection Performance in a Compact Package

UL Recognized, the new GDT225HE Series meets the reliability requirements of lightning-prone industrial, renewable energy and telecom applications

RIVERSIDE, Calif., February 24, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its GDT225HE Series High Voltage, High Energy Gas Discharge Tube (GDT) Arresters. Providing industry-leading surge protection performance in a compact package, Bourns® new GDTs are optimized for high-energy AC-DC power systems, including EV charging infrastructure, Battery Energy Storage Systems (BESS) and industrial power conversion equipment. These systems, in particular, are known to experience commutation or fault insertion events. It is the series’ ability to safely conduct prolonged high thermal (I²t) energy during transient conditions that makes it well-suited for system-level surge and fault protection, equipotential bonding and for lightning-prone designs where high-energy discharge must be safely diverted and controlled.

The Bourns® GDT225HE Series features a broad DC Breakdown Voltage (DCBV) from 1000 to 2000 V, In 40 kA (Nominal Discharge Current) and Imax 60 kA (Maximum Discharge Current) ratings on an 8/20 μs waveform to deliver exceptional protection for lightning-prone and high-energy applications. These high-power GDTs provide a space-saving alternative to bulky surge protection solutions by delivering very high current handling capabilities for AC power line applications in a small low-profile, reduced-volume and space-saving footprint. To help designers satisfy the requirements in today’s high-density and space-constrained PCB-based designs, this new series is also available in various lead shapes to fit in different configuration specifications.

The Bourns® GDT225HE Series is available now and is UL Recognized, ITU-T K.12 tested and RoHS compliant*. For additional information, please see: bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/high-voltage-series.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com