Search
Languages

Bourns Latest RF Inductors Deliver High Reliability from Advanced Multilayer Technology and Monolithic Construction

The four new multilayer chip inductor series are optimized for RF applications and deliver high-frequency performance with a compact, low‑profile design

RIVERSIDE, Calif., February 23, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced four Multilayer Chip Inductor Series: the CE0603G, CE0603M, CE1005Q, and CE1608Q Series. These new inductors feature a monolithic structure achieved through advanced multilayer technology giving power electronics designers a high-reliability, stable and superior signal integrity solution. These four series are available in compact form factors ranging from 1608 and 1005 down to the smallest 0603 mm, providing designers with more options in smaller sizes.

Helping to enable enhanced performance in high-frequency circuits, the new chip inductors feature high Self-Resonant Frequency (SRF) values of up to 20,000 MHz with tight inductance tolerance and rated current values from 100 to 1000 mA. All four high-SRF inductor series feature an operating temperature range from -55 to +125 °C, and have been optimized for use in RF amplifiers, low-voltage power supply modules, radio transmitters, radar, wireless communication and various mobile electronic devices.

Bourns® CE0603G, CE0603M, CE1005Q, and CE1608Q Series Multilayer Chip Inductors are available now and are RoHS compliant*. For more detailed product information, please see: bourns.com/products/magnetic-products/chip-inductors-multilayer.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com