Search
Languages

Bourns Introduces New Semi-Shielded Power Inductor Series with Polarity Control for Optimized EMI Suppression

New automotive grade, AEC-Q200 compliant SRN5040TA-P Series meets stringent temperature and reliability requirements for advanced automotive systems

RIVERSIDE, Calif., September 24, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its SRN5040TA-P Series of Semi-Shielded Power Inductors. The new series features polarity control that optimizes Electromagnetic Interference (EMI) protection for a wide range of automotive systems. These automotive grade, AEC-Q200 compliant semi-shielded power inductors provide excellent power management performance and thermal stability, meeting the demanding temperature and reliability requirements of advanced systems, including DC-DC converters, power supplies, driver assistance, infotainment and lighting systems.

The new SRN5040TA-P semi-shielded power inductors feature a specialized construction that minimizes magnetic field radiation while delivering high heating current and saturation current capabilities. In addition, the series supports a wide operating temperature range of -55 °C to +125 °C, making it ideal for space-constrained automotive applications. The semi-shielded design utilizes a magnetic-epoxy coating around the winding perimeter, providing effective EMI suppression and lower magnetic field radiation compared to non-shielded inductors.

The Bourns® SRN5040TA-P Series is available now through Bourns’ authorized distribution partners. It is RoHS* compliant and halogen** free. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk)†, audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com