Search
Languages

Bourns Announces Rugged, High-Power Thick Film Resistor Series Housed in a TO-247 Package

The Riedon™ PF2472 Series Power Resistors by Bourns deliver excellent thermal efficiency/high power capabilities from 100 W of heat-sinked power and up to 700 V operating voltage

RIVERSIDE, Calif., July 30, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its Riedon™ PF2472 Series Power Resistors by Bourns. Housed in a compact TO-247 package, this rugged, high-power thick film resistor family delivers 100 W of heat-sinked power and up to 700 V operating voltage, providing excellent thermal efficiency and in-demand high-power capabilities. It utilizes thick film technology, offering a high-reliability, compact and cost-effective solution for current limiting, current measurement, snubber circuits and capacitor discharge functions in industrial motor drives, power conversion and battery energy storage systems.

The Riedon™ PF2472 Series by Bourns features ultra-low inductance (<50 nH) and exceptional pulse handling, all with a precise ±1 percent tolerance across a wide resistance range from 0.1 ohms to 20k ohms. Of particular importance in many of today’s high-power density electronics, superior power dissipation is delivered in a single space-saving package that provides essential high-heat tolerance.

The Riedon™ PF2472 Series by Bourns is available now through Bourns’ authorized distribution partners, and is RoHS* compliant. For more detailed product information, please see: bourns.com/products/resistors/high-power-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com