Search
Languages

Bourns Announces High-Reliability Multilayer Common Mode Filters with Monolithic Construction that Uses Composite Co-Fired Materials

Bourns® CCF1206 Series Multilayer Common Mode Filters help enable complex circuit designs in compact devices and support efficient use of PCB space

RIVERSIDE, Calif., June 17, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its CCF1206 Series Multilayer Common Mode Filters that have a monolithic construction using composite co-fired materials. This advanced construction method allows for a smaller and highly reliable component design that supports more efficient PCB layouts. The advantages delivered with Bourns® new common mode filters support complex circuit designs in compact devices making them well-suited for high-speed differential signal transmission lines such as USB and LVDS as well as for MIPI serial interfaces in mobile devices.

Providing a superior solution without distortion for common mode interference suppression, the new series helps improve signal integrity. Bourns® CCF1206 Series Multilayer Common Mode Filters feature an operating temperature range of -40 to +85 °C, an impedance range of 67 to 120 ohms and are available in a compact 1.2 x 1.0 x 0.6 mm footprint.

Bourns® CCF1206 Series Multilayer Common Mode Filters are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/chip-inductors-common-mode.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com