Search
Languages

Bourns Announces High-Reliability Multilayer Common Mode Filters with Monolithic Construction that Uses Composite Co-Fired Materials

Bourns® CCF1206 Series Multilayer Common Mode Filters help enable complex circuit designs in compact devices and support efficient use of PCB space

RIVERSIDE, Calif., June 17, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its CCF1206 Series Multilayer Common Mode Filters that have a monolithic construction using composite co-fired materials. This advanced construction method allows for a smaller and highly reliable component design that supports more efficient PCB layouts. The advantages delivered with Bourns® new common mode filters support complex circuit designs in compact devices making them well-suited for high-speed differential signal transmission lines such as USB and LVDS as well as for MIPI serial interfaces in mobile devices.

Providing a superior solution without distortion for common mode interference suppression, the new series helps improve signal integrity. Bourns® CCF1206 Series Multilayer Common Mode Filters feature an operating temperature range of -40 to +85 °C, an impedance range of 67 to 120 ohms and are available in a compact 1.2 x 1.0 x 0.6 mm footprint.

Bourns® CCF1206 Series Multilayer Common Mode Filters are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/chip-inductors-common-mode.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf