Search
Languages

Bourns Adds Four New Product Series to its Shielded Power Inductor Portfolio

New shielded power inductors feature high heating/saturation current and low magnetic field radiation

RIVERSIDE, Calif., April 29, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today added four new product series to its line of shielded power inductors. The Bourns® SRP4021HMCT, SRP4021HMT, SRP5030HMCT, and SRP5030HMT Shielded Power Inductor Series feature high heating and saturation current with low magnetic field radiation to deliver enhanced power handling, increased efficiency, and optimized power circuit filtering.

The new shielded power inductors are produced with a hot press molding process that matches design needs for inductive components with greater density and additional mechanical strength. Compared to the previous Bourns® SRP series, the electrical characteristics have been enhanced by approximately 20 percent. This improvement is reflected in parameters such as the series’ higher current rating, lower DCR, and reduced power loss. The result is that Bourns is able to offer a smaller size inductive solution while maintaining the same electrical performance.

The Bourns® SRP4021HMCT, SRP4021HMT, SRP5030HMCT and SRP5030HMT Shielded Power Inductor Series are available now from Bourns’ authorized distribution partners, and are RoHS* compliant. For more detailed product information, please see: /bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com