Search
Languages

Bourns Launches Automotive Grade Multilayered Varistor Series with Advanced Transient Energy Absorption for Superior Surge Protection

Specifically designed for automotive circuits, new varistors deliver enhanced energy volume distribution and power dissipation available in 1210 and 1812 SMD packaging

RIVERSIDE, Calif., April 22, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today launched two new product series additions to its automotive grade, AEC-Q200 compliant BVRA multilayered varistor line. Bourns specifically designed its new BVRA1210 and BVRA1812 Series to deliver superior surge protection for today’s increasingly sensitive automotive circuits. These low voltage multilayer varistors feature excellent transient energy absorption due to their state-of-the-art energy volume distribution and advanced power dissipation design.

The varistor additions to the BVRA line meet IEC 61000-4-5 standard requirements, giving automotive designers the effective overvoltage protection needed to safeguard components from harmful transient voltage events. Offering exceptionally fast transient response (< 1.0 ns reaction time), these varistors help to ensure prompt energy diversion during surge events. Plus, the new series provide stable leakage current for consistent overvoltage protection, and are available with a wide working voltage range from 11 V to 100 V DC. The optimized design of both new BVRA series are available in compact SMD EIA 1210 and EIA 1812-size packaging with the added benefit of an insulator overcoat that aids in streamlining integration while enhancing efficiency.

The Bourns® BVRA1210 and BVRA1812 Series are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and lead free. For more detailed product information, please see: bourns.com/products/circuit-protection/varistor-products/mlv.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com