Search
Languages

Bourns Launches Three Automotive Grade Chip Inductor Series Featuring High Current and High Inductance in a Miniature Size

Bourns® CWF1610A, CWF1612A, and CWF2012A Series deliver excellent power handling and filtering at high frequency

RIVERSIDE, Calif., April 7, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its CWF1610A, CWF1612A and CWF2012A Series chip inductors. These AEC-Q200-compliant, automotive-grade inductors feature high inductance, high current and high self-resonant frequency in a compact form factor. The features enable excellent power handling and filtering at high frequency, making the three new chip inductor series superior power conversion solutions in RF signal processing, resonant circuits, decoupling, noise filters and low current DC power lines found in a broad variety of automotive, power, audio and mobile designs.

The CWF1610A, CWF1612A, and CWF2012A Series all have wirewound construction on a ferrite core to provide minimal resistance and exceptional noise filtering across a wide frequency range. As an example, the CWF1610A Series offers saturation current from 200 mA up to 1700 mA, rated current from 200 to 1400 mA, and an extended operating temperature range of -55 to +125 °C.

The Bourns® CWF1610A, CWF1612A and CWF2012A Chip Inductor Series are available now through Bourns’ authorized distribution partners and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/chip-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com