Search
Languages

Bourns Introduces AEC-Q200 Compliant Automotive Grade Chip Inductor Series as Space-Saving Solution for Power over Coax Circuits

Bourns® Model CWP3230A Series features high current, inductance and impedance in a compact form factor

RIVERSIDE, Calif., June 6, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its Model CWP3230A Series chip inductors. These AEC-Q200 compliant automotive grade inductors feature high current, inductance and impedance in a compact form factor. The new series’ high impedance and current capabilities make them ideal for applications using coaxial cable, where both power and video signals are simultaneously transmitted. Bourns® Model CWP3230A Series enables designers to decrease the number of inductors and chip beads in circuit, to save space and reduce development costs.

The CWP3230A Series is designed with a ferrite powder core, and bifilar and trifilar windings to achieve a higher saturation current and heating current level in a small size. The series has an inductance range of 2.2 - 47 µH and an operating temperature range of -50 to +150 °C. These features are required in a growing variety of space-constrained ADAS applications that must also meet lower power consumption goals such as in Power over Coax (PoC) vehicle camera modules.

The Bourns® Model CWP3230A Chip Inductor Series is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/chip-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com