Search
Languages

Bourns Announces Two AEC-Q200 Compliant, Automotive Grade Common Mode Chip Inductor Series

Bourns® Model SRF4532TA withstands current up to 4 A in a compact size; Model SRF3225TABG meets Open Alliance 1000Base-T1 Automotive Ethernet requirements

RIVERSIDE, Calif., May 2, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced two new AEC-Q200 compliant, automotive-grade common mode chip inductor model series. Bourns® Model SRF4532TA is designed to withstand current up to 4 A, and Bourns® Model SRF3225TABG meets Open Alliance 1000Base-T1 Automotive Ethernet requirements. These common mode chip inductors are ideal as noise suppression solutions in Advanced Driver-Assistance Systems (ADAS) infotainment, body electronics, and many other automotive applications. The Model SRF3225TABG is specifically designed for noise suppression in 1000Base-T1 Ethernet applications.

Offered in a compact footprint, both common mode chip inductor model series are designed with a ferrite core, providing high impedance across a broad frequency range to suppress unwanted incoming or outgoing EMI signals. These common mode chip inductors address stringent shock and vibration requirements, as the core is constructed with 0.3/0.4 mm high sidewall terminals that help to enhance the component's mechanical strength on the PCB. The Model SRF4532TA and SRF3225TABG Series also feature shielded construction for low radiation and have an operating temperature range of -55 to +125 °C and -40 to +125 °C, respectively.

The Bourns® Model SRF4532TA and SRF3225TABG Series are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chip-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com