Search
Languages

Bourns Announces Zero Ohm High Power Jumper Resistor Series Offering Very Low Resistance Values

Featuring a high current rating and a robust metal strip element, Bourns® AEC-Q200 compliant jumpers enable designers to connect separated points on a PCB

RIVERSIDE, Calif., January 29, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the Model CRF Series High Power Metal Strip Jumper. Also known as zero ohm resistors, jumpers feature very low resistance values, and are used to connect separated points that cannot be connected via printed traces on a PCB. Compared to thick film jumpers, Bourns' new AEC-Q200 compliant high power jumpers offer a higher current rating and lower resistance, making them well-suited for broad range of consumer, industrial, telecommunication and automotive designs.

Bourns® new Model CRF Series zero ohm jumpers are manufactured using copper alloy with a protective overcoat material, and are offered in four different footprint sizes; 0805, 1206, 2010 and 2512, and provide a maximum resistance value of 0.2 milliohms. They feature a high current rating up to 100 A, an operating temperature range of -55 °C to +150 °C and are available in tape and reel packaging.

The Bourns® Model CRF Series high power metal strip jumper is available now. These models are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/resistors/fixed-resistors-aec-q200-compliant-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com