Search
Languages

Bourns Announces AEC-Q200 Compliant, Automotive Grade Shielded Power Inductors with Wide Operating Range

Constructed with bottom-soldered lead wire, these new inductors' enhanced mechanical strength and stability provide increased product reliability

RIVERSIDE, Calif., January 11, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its new automotive grade Model SRR0735HA and SRR0745HA Series High Temperature Shielded Power Inductors. These power inductors are designed with a ferrite core and ferrite shield for low magnetic field radiation, making them ideal for low noise operating environmental applications such as in automotive driver assistant devices, infotainment systems and lighting designs.

The Model SRR0735HA and SRR0745HA Series are AEC-Q200 compliant and automotive grade, and feature a broad operating temperature range of -55 °C to +150 °C. In addition to automotive systems, the extended capabilities of Bourns' new auto grade inductors are also superior solutions to meet higher reliability requirements in DC-DC converters and power supplies in consumer, industrial and telecom applications.

Bourns® Model SRR0735HA and SRR0745HA High Temperature Shielded Power Inductor Series are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com