Search
Languages

Bourns Launches Automotive Grade Semi-shielded Power Inductor Series Featuring High Operating Temperatures Up to 150 °C

AEC-Q200 compliant inductor series is constructed with magnetic silicon-based coating technology for superior magnetic shielding and supports higher operating temperatures

RIVERSIDE, Calif., June 22, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new AEC-Q200 compliant, automotive grade semi-shielded power inductor series that features a high operating temperature range from -40 °C up to 150 °C. The Bourns® Model SRN8040HA Series is constructed using the company's advanced magnetic silicon-based coating technology that offers superior magnetic shielding while also enabling higher operating temperatures.

Bourns' new high temperature inductors are designed to release lower magnetic field radiation compared to non-shielded inductors, and are also a more cost-efficient alternative to fully shielded ferrite-based inductors. The Model SRN8040HA series supports high current capacity with saturation current Isat ranging from 1.3 – 15 A and provides a heating current Irms range of 1.0 – 10.0 A. The features and capabilities of these inductors make them especially well-suited for DC-DC converters and power supplies in automotive, consumer, industrial, and telecom electronics applications where greater inductor reliability is a frequent requirement.

The Bourns® Model SRN8040HA semi-shielded power inductor series is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded/product/SRN8040HA

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com