Search
Languages

Bourns Unveils Bourns' Highest Current Carrying PTVS Diode Series in a Compact DFN Package

New bidirectional PTVS diode family features 20 kA, 8/20 µs surge handling capability with low clamping voltage designed for high power DC line applications

RIVERSIDE, Calif., January 4, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released Bourns' highest current carrying bidirectional Power Transient Voltage Suppressor (PTVS) Diode series that is available in a compact surface mount DFN package. Bourns® Model PTVS20-015C-H is capable of handling 20 kA, 8/20 µs current surge at a low voltage of 15 V. These features deliver effective electrostatic discharge (ESD) protection in applications that require high power DC line protection.

The Bourns® Model PTVS20-015C-H PTVS Diode meets IEC 61000-4-2 Level 4 ESD protection requirements. It also features low clamping voltage at peak pulse current and assists in meeting IEC 61000-4-5 8/20 μs current surge requirements for lightning protection.

In order to support large currents such as 60 kA in next-generation applications, designers typically have had to connect many devices with low current handling capability in parallel. With a single device capable of handling 20 kA, a fewer number of devices can now be connected in parallel to achieve the same desired protection level. This reduces the total BOM count and can help save valuable space on the PCB.

The Bourns® Model PTVS20-015C-H is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/diodes/power-tvs-diodes

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com