Search
Languages

Bourns Announces New Non-Contacting Feedback Rotary Sensor with SSI Output

New Model DMS22B is designed to meet heavy-duty application specifications for long cycle life and high reliability

RIVERSIDE, Calif., May 3, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its latest non-contacting feedback rotary sensor that features Synchronous Serial Interface (SSI) output providing effective synchronization in closed-loop control systems. This single-turn rotary sensor is based on Hall Effect technology and is supported by a factory programmable electrical angle from 10 to 360 degrees that enables more consistent and dependable operation of up to 50 million shaft revolutions.

The Bourns® Model DMS22B rotary sensor is designed with non-contacting magnetic technology offering consistent excellent performance and high reliability that is well-suited for a range of application environments. Plus, its IP50 seal rating makes this rotary sensor highly resistant to fluid/dust ingress. Available with a 7/8-inch flatted shaft and bushing mount configuration, the Bourns® Model DMS22B rotary sensor offers designers a highly versatile position sensing solution for a broad variety of applications including patient platform positioning feedback, pneumatic control valve position feedback, draw wire position sensors, remote communications antenna positioning, actuator motor position feedback, automated manufacturing robotics and more.

The Bourns® Model DMS22B rotary sensor is available now and is RoHS* compliant. For more detailed product information, please see: www.bourns.com/products/sensors/position-sensors/non-contacting-single-turn

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com