Search
Languages

Bourns Further Expands its Discrete TVS Diode Product Line

RIVERSIDE, Calif., October 21, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the further expansion of its industry-leading line of discrete transient voltage suppressor (TVS) diode products with two new series of ESD/EFT surge protection products. Bourns designed its Model SMA6J and Model SMA6J-Q TVS diodes to protect power buses and I/O interfaces in data lines and DC power supplies. In addition, Bourns® Model SMA6J-Q is AEC-Q101 compliant and well-suited for a broad range of communications, industrial and consumer electronics applications that are used in certain harsh environments and require high reliability.

Both model series come in a compact, industry standard DO214-AC (SMA) package, and feature increased peak pulse power (PPP) dissipation of 600 watts compared to the 400-watt industry standard. TVS diodes are typically rated for peak pulse power allowing designers to determine the best type required for a particular application and environment. These unidirectional/bidirectional devices offer reverse standoff voltage of 5 – 43 V. The features of Bourns' new TVS diodes help enable power supply designers to meet their both their high-power density and small form factor requirements.

Bourns® Models SMA6J and SMA6J-Q are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/diodes/diodes-aec-q101-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com