Search
Languages

Bourns to Demonstrate Broad Breadth of Standard and Custom Component Solutions for Power Applications at PCIM 2018

RIVERSIDE, Calif., May 8, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, will showcase its broad passive component line and extensive expertise in high power, high frequency magnetics design at PCIM 2018.

Booth highlights:

  • Demonstrations:
    • Bus bar 1000 A 50 µOhm current sense resistor that provides accurate measurement of 500 A or more due to precision ultra-low resistance combined with low offset high common mode voltage current sense circuit
    • AEC-Q200 compliant Ethernet transformers with high inductance values and high working voltages optimized for BMS designs
    • High-voltage 550 V TBU® high-speed protectors that deliver 150 mA trip currents, and 1 µs reaction times to protect battery monitor lines during hot swapping or from transients
    • SinglFuse™ products rated to 125 V DC for short circuit protection on battery monitor lines
  • Low 0.8 milliohm resistance, 30 A DC current-rated flat wire inductor for 48 V converters
  • Transformers for multiple kilowatt full bridge LLC converters complete with Litz wire and reinforced insulation
  • Power TVS Diodes for clamping flyback voltages caused by short circuit events

Where: PCIM, Nuremberg Messe, Germany
When: June 5 – 7, 2018
Location: Bourns Booth #147, Hall 7

To learn more about how Bourns is enabling advancements in battery management electronics, we invite you to speak with a Bourns representative. To schedule a meeting, please contact Annette Keller: +1 707-947-7232, annettekeller@sbcglobal.net.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com