Search
Languages

Bourns Partners with Mouser Electronics for Special Promotion at 2017 NAMM Show

RIVERSIDE, Calif., January 16, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that it has exclusively partnered with Mouser Electronics to promote their industry-leading Pro Audio and Pro Lighting products including the latest PTL01 and PSP01 slide potentiometers at the 2017 NAMM Show.

Bourns will be giving away a Zemaitis C24MF Custom Metal Top Guitar with a Floyd Rose FRX surface-mount tremolo system, Bourns Sean Silas Signature Series Guitar Potentiometers, locking tuners, and other custom upgrades. Stop by the Bourns booth in Hall A, #6861 to see and enter for a chance to win this amazing custom guitar. No purchase is required and all entries are subject to contest rules.

The Bourns® Model PTL01 100 mm slide potentiometer with LED is an optimal solution for level controls in audio mixing, light mixing, and broadcast consoles, or for sound processors. Bourns designed its Model PSP01 motorized master slide potentiometer with an extended cycle life of up to 1 million cycles making it exceptionally well suited for automated Pro Audio mixing consoles, broadcast consoles and Pro Lighting consoles/controllers.

With a commitment to excellence and delivering advanced technology, Bourns supports the professional audio industry with quality, high reliability and value-added products. The company's established customer base that includes some of the industry's leading manufacturers and suppliers of audio and lighting equipment.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk)†, audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com