Search
Languages

Bourns Introduces Bidirectional Thyristor Surge Protectors Offering Very Low Breakover Voltage

RIVERSIDE, Calif., November 22, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has expanded its leading line of bidirectional overvoltage protectors offering very low breakover voltage. Designed to limit damaging overvoltage threats, Bourns latest thyristor surge device provides optimized 2-point protection for transformer windings, low voltage electronics and digital telecommunication lines.

The Bourns® Model TISP4011H1BJ, as with other members of the Model TISP40xxH1BJ series, features very low V(bo) breakover voltage of 10.5V, which allows designers to protect lines of working voltages up to 5.25V. Delivering excellent protection for electrical overstress (EOS) conditions, both models provide low voltage overshoot and low capacitance. Offering a space-saving design, these overvoltage protectors are symmetrical voltage-triggered bidirectional thyristors housed in a surface mount SMB package.

Pricing and Availability
As a pricing reference, the Bourns® Model TISP4011H1BJ is priced at $0.30 each in 12,000 piece quantities. It is available now and is RoHS compliant* and halogen free**. For additional product information, please see: www.bourns.com/products/circuit-protection/thyristor-surge-protectors/tisp4xxxhx-single-bidirectional-thyristor-surge-protector

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be “halogen free” if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com