Search
Languages

Bourns Maintains Leading AEC-Q200 Component Supplier Position with Introduction of Semi-Shielded and Shielded Power Inductor Series

Bourns’ AEC-Q200 Certified Semi-shielded Power Inductors
Click to enlarge (477 KB)

RIVERSIDE, Calif., ​September ​6, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a broad new series of automotive-grade semi-shielded and shielded power inductor components. Bourns offers one of the industry's broadest portfolios of AEC-Q200-qualified products consisting of resistors and magnetics that condition and filter electronic circuits, and circuit protection products designed specifically for automotive applications. AEC-Q200 is a global automotive standard for passive components to ensure temperature, pressure resistance and safety consistency. Along with the entire line of Bourns' automotive-grade components, the nine new inductor series have been tested and qualified to the AEC-Q200 specification, and are manufactured in facilities that are fully certified to TS 16949.

"Based on specific requests from our automotive market customers for semi-shielded inductors, the products were developed and tested, and are being manufactured according to strict AEC-Q guidelines in TS certified factories,” said Guido Zehnder, product line manager at Bourns, Inc. "Automotive designers can be assured of a component that has passed very clear defined specifications with dedicated controls.”

Bourns released six new AEC-Q200-qualified semi-shielded power inductor series: SRN2010TA, SRN3012TA, SRN3015TA, SRN4012TA, SRN6045TA and SRN8040TA and three AEC-Q200-qualified shielded power inductor series: SRR1050A, SRU1063A and SRU8045A. These inductors have been designed to provide effective magnetic shielding with low radiation, feature extended temperature range (-40 to +125 °C) operation and offer cost-effective solutions compared to similarly-sized conventional ferrite shield inductors. These features make them ideal for applications where low noise operating environments are essential such as driver assistant devices, information/entertainment systems, lighting as well as DC/DC converters and power supplies.

Pricing and Availability
Bourns' new series of semi-shielded and shielded power inductor components are available now and are RoHS compliant*. As a pricing reference, the semi-shielded Model SRN3012TA is priced at $0.12 each in 10,000 piece quantities and the shielded Model SRR1050A is priced at $0.40 each in 10,000 piece quantities. For additional product specifications, please go to: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-qualified

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com