Search
Languages

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com