Search
Languages

Bourns Announces Enhanced Temperature Performance High Power TVS Diodes for AC/DC Power Line Applications

Riverside, Calif., February 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced new high power TVS diodes for use in DC bus protection applications. The new models deliver high current bidirectional port protection that meets IEC 61000-4-5 8/20 µs current surge requirements and are RoHS* compliant. Designated Bourns® Models PTVS6-058C-TH and PTVS6-076C-TH, this new series of power TVS diodes provide enhanced temperature performance for greater system stability and increased reliability. Designed using advanced silicon technology, Bourns' new devices offer lower clamping voltage under surge compared to Metal Oxide Varistor (MOV) technology. In Bourns' testing, the new models have exhibited an excellent surge response versus temperature; the typical maximum surge current at 150 °C 75 % of their rated value at 25 °C.

"We designed Bourns' two new high power TVS diodes with enhanced temperature performance to meet robust circuit protection requirements that offer superior protection against power line surges and indirect lightning strikes in AC and DC power line applications," said Ben Huang, Semiconductor Product Line Manager at Bourns, Inc. "Our new diode series also provides excellent surge performance and temperature ratio benefits that are critical requirements in today's demanding high power applications."

Both Bourns® models provide very high surge current protection with a peak pulse current rating of 6 kA. The Bourns® Model PTVS6-058C-TH features a 58 V standoff voltage and the Bourns® model PTVS6-076C-TH has a 76 V standoff voltage.

Pricing and Availability
As a pricing reference, the Bourns® models PTVS6-058C-TH and PTVS6-076C-TH are priced at $13.78 each in 10 piece quantities and $12.60 each in 500 piece quantities, respectively. Both models are available now. For additional product specifications, please go to: www.bourns.com/docs/product-datasheets/PTVS6-TH.pdf.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com