Search
Languages

Bourns® New AEC-Q200 Compliant, Automotive Grade Thin Film Chip Resistors Offer Higher Resistance Tolerance Accuracy and TCR

Bourns® Model CRT-A Series meets growing demand for small, accurate resistance resistors in automotive, mobile phone, SD card, DDR memory and camera module applications

RIVERSIDE, Calif., August 22, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its AEC-Q200 compliant, automotive grade thin film chip resistor model series. The Model CRT-A Series provides higher resistance tolerance accuracy and Temperature Coefficient of Resistance (TCR) compared to traditional through-hole type resistors. The new series delivers enhanced signal quality and is offered in an SMD package. These compact, yet high power-rated resistors offering accurate resistance levels are increasingly required in space-constrained applications, such as mobile phones, SD cards, DDR memory modules and camera modules. Designed to automotive-grade standards, Bourns® CRT-A Series resistors are also ideal resistive solutions for a variety of automotive applications.

This latest thin film resistor series is available in 0402, 0603, 0805 and 1206 package sizes, supports lower tolerances from 0.1 to 1 percent and features a wide TCR range from ±50 PPM/°C to ±10 PPM/°C. In addition, the series provides a resistance range from 10 Ω to 1M Ω and TCR down to ±10 PPM/°C.

The Bourns® Model CRT-A Series is available now and is RoHS* compliant and sulfur- resistant. For more detailed product information, please see: www.bourns.com/products/resistors/fixed-resistors-aec-q200-compliant-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com