Search
Languages

Bourns Introduces Thermal Jumper Chip Series that Provides an Excellent Thermal Dissipation Solution in a Compact Form Factor

The high thermal conductivity and insulating properties of Bourns® BTJ Series Thermal Jumpers help protect and prolong system component lifespan

RIVERSIDE, Calif., December 18, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its BTJ Series Thermal Jumper Chips designed to provide effective thermal dissipation in a compact form factor.. These unique devices provide high thermal conductivity while also having insulating properties to help protect and prolong system component lifespans. Because the thermal jumper chips are able to quickly dissipate heat and do not conduct electricity, they have no impact on system operation.

Available in SMD packaging, Bourns® new Thermal Jumper Chips provide an excellent thermal dissipation solution for a variety of mobile devices and electronic equipment that include power supplies, converters and RF and GaN amplifiers.. Furthermore, the advanced design takes advantage of the chips' insulating properties so the space between the heating element and the heat detection element can be filled to enable highly accurate heat detection. These features also help reduce the temperature rise of key components contributing to improved reliability at the system level.

The Bourns® BTJ Series Thermal Jumper Chips are available now and are RoHS* compliant and halogen free**. For additional product information, please see: bourns.com/products/thermal-solutions/thermal-dissipation-devices.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com