Search
Languages

Bourns Introduces 21-Model TVS Diode Series that Delivers a Wide Peak Voltage Range for Additional Design Flexibility

New series offers advanced capabilities that provide effective ESD protection and is available in compact unidirectional and bi-directional package options

RIVERSIDE, Calif., November 17, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its SMLJ-R Series Transient Voltage Suppressor (TVS) Diodes. Designed with high performance energy absorption and clamping capabilities that provide effective Electrostatic Discharge (ESD) protection for sensitive electronics, this new series is available in compact DO-214AB packaging with unidirectional and bi-directional options. The capabilities and packaging offered make these TVS Diodes superior surge protection solutions for portable communications, computing and video equipment applications.

The Bourns® SMLJ-R Series TVS Diodes provide additional design flexibility with a choice of working peak reverse voltage from 12 V to 30 V and a power dissipation of 3000 watts. Designers can also select from 13 unidirectional part numbers and eight part numbers with bi-directional structures. The series has also been tested to comply with IEC 61000-4-2 ESD (Min. Level 4), IEC 61000-4-4 EFT and IEC 61000-4-5 Surge standards.

The Bourns® SMLJ-R Series TVS Diodes is available now through Bourns’ authorized distribution partners and is RoHS* compliant. For more detailed product information, please see: bourns.com/products/diodes/tvs-diodes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com