Search
Languages

Offering High Current and Impedance Over a Broad Frequency Range, Bourns Releases Two High Current Common Mode Choke Models

New automotive grade, AEC-Q200 compliant models provide effective EMI suppression and noise filtering solutions for power line and automotive system applications

RIVERSIDE, Calif., September 15, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released two new high current common mode choke models, the SRF1206A-501Y and SRF1206A-172Y. Designed to provide more impedance and current options for designers, these models are an extension of Bourns® AEC-Q200 compliant, automotive grade SRF1206A Series. These chokes offer high impedance over a broad frequency range to provide an effective EMI suppression and noise filtering solution for in-vehicle switch-mode power supplies in addition to other automotive, consumer and industrial systems.

These two new common mode choke models feature a monolithic ferrite core with a closed-loop magnetic path, offering excellent magnetic shielding performance. They are constructed with a sector-wound configuration that helps enhance dielectric strength between windings. The impedance range of these two models extends from 500 to 1700 ohms (Ω), with current ratings up to 10 A and an operating temperature range from -40 to +125 °C.

The Bourns® SRF1206A-501Y and SRF1206A-172Y automotive grade, AEC-Q200 compliant common mode chokes are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/common-mode-chokes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com