Search
Languages

Bourns® IsoMOV® Hybrid Protectors Earn IEC 61051-2 Certificate of Conformity and are UL 1449 Listed

With features that extend application service life and enhance reliability, IsoMOV® protectors are the first hybrid surge protection devices to receive both global standards

RIVERSIDE, Calif., May 1, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its innovatively designed IsoMOV® hybrid protectors have earned the IEC 61051-2 Certificate of Compliance and are UL 1449 listed. Bourns® IsoMOV® protectors are the first hybrid surge protection devices to have met the stringent tests and documentation required by these global standards. Now, designers can confidently add the longevity and high reliability benefits IsoMOV® protectors provide to a growing group of key market applications where IEC certification is a prerequisite.

“Earning the IEC Certificate of Conformity is a significant achievement for Bourns, enabling our valued customers to benefit from the extended lifespan and enhanced reliability of our IsoMOV® protectors across a wider range of designs. The comprehensive documentation required to validate this innovative solution—especially in the absence of an existing IEC standard for hybrid overvoltage protection components—highlights our product team's commitment to delivering top-tier solutions that give our global customers a competitive edge," said Craig Shipley, President of the Bourns Protection Division.

The Bourns® IsoMOV® protector is a fully integrated GDT and MOV hybrid design that combines both devices into a single package, allowing the GDT to block leakage currents through the MOV that may lead to premature failure. It provides an elevated level of surge protection in terms of performance, operational life and enhanced device reliability. Because this compact hybrid design features performance specifications usually found in larger traditional MOV devices, Bourns® IsoMOV® protectors enable designers to better tailor the surge protection performance to their stringent space requirements.

Bourns® IsoMOV® hybrid protectors are available through Bourns’ authorized distribution partners and are RoHS* compliant. For more detailed product information, please see: bourns.com/products/circuit-protection/isomov.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com