Search
Languages

Bourns Introduces Dual-Winding Shielded Power Inductor Series as Space-Saving, Cost-Efficient Solution for Noise Filtering Applications

Offering exceptional rated current and inductance design versatility, new AEC-Q200 compliant, automotive grade inductors can be used in parallel, series, dual-inductor or transformer configurations

RIVERSIDE, Calif., January 9, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its Model SRF0703HA Series Dual-Winding Shielded Power Inductor Series. Bourns® new AEC-Q200 compliant, automotive grade power inductors can be used in parallel, series, dual-inductor or transformer configurations, giving designers outstanding rated current and inductance versatility. In addition, the single package dual-winding inductors provide a space-saving and cost-efficient solution compared to using two individual inductors.

Delivering a superior solution for Single-Ended Primary Inductance Converter (SEPIC) topologies, automotive systems and power supplies, the Model SRF0703HA series features a broad operating temperature range of -55 °C to +150 °C. These power inductors also are magnetically shielded to provide low radiation, which is especially important for applications that need to adhere to reduced noise requirements.

The Bourns® Model SRF0703HA Dual-Winding Shielded Power Inductor Series is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-dual-winding-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com