Search
Languages

Bourns Introduces SMD Wirewound Resistor Series that Features High Power Ratings and High Pulse Withstanding Capabilities

The latest Model PWR Series helps meet increased reliability and stability requirements for discharge/pre-charge circuits in solar power and motor control applications

RIVERSIDE, Calif., January 6, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its latest family of SMD wirewound resistors. Featuring high power ratings (up to 10 W) and high pulse withstanding capabilities, the Bourns® Model PWR6927/8030/8937/A247/B053 Series is designed to help designers meet the increased reliability and stability required in discharge and pre-charge circuits used in solar power, motor control, telecommunication, Switched-Mode Power Supply (SMPS), and Energy Storage System (ESS) applications.

Based on the series’ advanced SMD architecture and its higher surge withstanding capability, Bourns’ new family of wirewound resistors delivers a lower inductive solution that reduces interference with magnetic fields compared to standard through-hole, thick film resistors, thin film resistors, and conventional wirewound resistors. In addition, the models in this series are UL 94V-0 and Substances of Very High Concern (SVHC) compliant that aid in meeting various application safety requirements.

The Bourns® Model PWR6927/8030/8937/A247/B053 Series is available now and is RoHS* compliant with a halogen free** option. For more detailed product information, please see: www.bourns.com/products/resistors/wirewound-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com