Search
Languages

Bourns Expands its POWrFuse™ High-Power Fuse Product Family with New Semiconductor (Class aR) Model Series

Latest Bourns® POWrFuse™ High-Power Fuse models are specifically designed to meet UL 248-13 standard for high power, high interrupting and high current rating applications

RIVERSIDE, Calif., June 30, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the expansion of the Company’s POWrFuse™ High-Power Fuse product family. The two new POWrFuse™ model PF-F and PF-M series are high power rating industrial fuse links specially designed to meet the UL 248-13 semiconductor (aR) standard. These high power fuses are excellent solutions to help protect sensitive power semiconductor devices against overcurrent events in a variety of power inverters, converters, rectifiers, AC/DC drives, UPS systems and reduced voltage motor starters.

The Bourns® POWrFuse™ PF-F series features 800 VAC/VDC voltage, power ratings from 50-400 A and up to a 100 kA @ 800 VAC and 50 kA @ 800 VDC interrupting rating. The POWrFuse™ PF-M series provides 240 VAC/150 VDC voltage, power ratings from 50-180 A and up to a 160 kA @ 240 VAC and 50 kA @ 150 VDC interrupting rating. Both of these high-power fuse series are bolt mounted, offer fast-acting protection under fault current, low resistance and power loss, and deliver an operating temperature range of -55 to +125 °C.

In addition, both series are UL recognized to help OEMs save qualification time while also enhancing overall quality and reliability. These attributes, in turn, help to lower the total cost of ownership for end customers.

The Bourns® POWrFuse™ model PF-F and PF-M series are available now and are RoHS compliant* and halogen free**. For more detailed product series information, please see: www.bourns.com/products/fuses/powrfuse-high-power-fuses

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com