Search
Languages

Bourns Introduces New AEC-Q200 Compliant High Current Shielded Power Inductor Series

New series features high rated current, low radiation, low DC resistance, low buzz noise and wide operating temperature range

RIVERSIDE, Calif., March 16, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced three new AEC-Q200 compliant high current shielded power inductor series. Helping to meet the high current density, high temperature and reliability requirements for power management and EMI filtering in a variety of consumer, industrial and telecom electronics applications, Bourns® Model SRP1580CA, SRP1510CA and SRP1513CA inductors offer high current capacity, compact size, high operating frequency and a high operating temperature range.

The three new AEC-Q200 compliant inductor series are manufactured with flat wire and Bourns' uniquely formulated metal alloy powder core using a molded construction manufacturing process. This process enables a superior magnetically shielded construction that offers low DC resistance, high heating / saturation current, low buzz noise and excellent temperature stability for low magnetic field radiation. In addition, all of the new models are built with flat enameled coated wire with self-lead terminal for ultra-low DC resistance. Plus, the new high current shielded inductors have an operating temperature range of -55 to +155 °C, and are designed with the same 16.5 x 15.5 mm interchangeable footprint.

The new Bourns® Model SRP1580CA, SRP1510CA and SRP1513CA series are available now and are RoHS compliant* and halogen free**. For additional product information, please see: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com