Search
Languages

Bourns Introduces AEC-Q200 Compliant CANbus Inductor Series

New SRF4530A Series Common Mode Chip Inductors are Optimal Noise Suppression Solutions for a Broad Range of High Temperature Electronics Applications

RIVERSIDE, Calif., August 3, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a new CANbus Common Mode Chip Inductor series. The new AEC-Q200 compliant inductors feature a ferrite core with a bifilar-wound construction that provides high impedance over a broad frequency range to suppress unwanted incoming or outgoing EMI signals.

Offered in a compact form factor, the SRF4530A series features a wide operating temperature range from –55 to +150 °C, an inductance range of 11 – 100 µH and an impedance range of 600 – 7500 Ω. Bourns designed its latest inductor series to meet noise suppression, high temperature operation and high reliability application requirements that are needed in many CANbus-based applications.

Bourns® SRF4530A series is available now and is RoHS* compliant. For additional product information, please see: www.bourns.com/docs/Product-Datasheets/SRF4530A.pdf

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com