Search
Languages

Bourns to Exhibit Latest Environmental Sensors for Medical Applications at MD&M West 2020

RIVERSIDE, Calif., February 4, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components will display its advanced MEMS-based environmental sensors at the MDM West 2020 conference. Bourns' growing line of pressure and humidity sensors is designed to meet the sensitivity, accuracy and long-term reliability requirements of certain medical market applications.

Sensors have become a critical component of information collection. With decades of experience in delivering proven circuit protection and magnetics solutions for portable, diagnostic and lab analysis equipment, the new MEMs-based sensor line from Bourns delivers the sensitivity, accuracy and long-term reliability required for many medical market applications.

Booth highlights:

  • High accuracy, ultra-low pressure range capabilities
  • New digital output features to help reduce processor workloads
  • High reliability operation over a broad -40 °C to +150 °C temperature range
  • Demonstration of ultra-low differential pressure sensors
  • Non-contacting rotary position sensors for diagnostic equipment

Where: MD&M West, Anaheim, CA
When: February 11–13, 2020
Location: Bourns Booth, Hall E, #963

You are invited to stop by the Bourns booth to learn more about the Bourns® Precision Sensors (BPS) for medium/low-risk medical* designs including portable oxygen generators, nebulizers, CPAP equipment, diagnostic spirometers and gas chromatography equipment.

*Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com