Search
Languages

Bourns New Bridge Rectifier Diode Series Offers Industry-Leading Capabilities Enabling More Power-Efficient Designs

RIVERSIDE, Calif., December 6, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced five new bridge rectifier product series designed for power and Switch-Mode Power Supply (SMPS) applications. The newly released products come in ultra-low profile packages of 1.0 mm to 1.4 mm making them well-suited for use in high-density board designs, and also for mounting onto the bottom side of Printed Circuit Board Assemblies (PCBAs) where necessary.

The Bourns® Model CD-MBL and Model CD-DF4 bridge rectifiers offer exceptional high forward current and low forward voltage making them optimum solutions for converting Alternating Current (AC) to Direct Current (DC) in power applications. These features allow designers to meet compact, high efficiency design requirements avoiding the need to specify larger diodes for higher current applications. Similarly, Bourns® Model CD-HD Schottky bridge rectifiers provide exceptionally low forward voltage in a space-saving package enabling developers of set-top boxes, monitors, cable modems and other AC-operated products to achieve power-efficient designs.

Pricing and Availability
All five new bridge rectifier series (CD-MBL1xx, CD-MBL2xx, CD-DF4xx, CD-HD0x Series and CD-HD2x) from Bourns are available now and are RoHS compliant*. As a pricing reference, the Bourns® Model CD-MBL series are priced from $0.14 (to $0.23) in 12,000 piece quantities, the Model CD-DF series is priced from $0.40 (to $0.50) in 12,000 piece quantities, and the Model CD-HD series are priced from $0.24 (to $0.48) in 15,000 piece quantities. For additional product information, please see: www.bourns.com/products/diodes/rectifier-diodes

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com