Search
Languages

Bourns Announces New Semi-Shielded Power Inductor Series for DC/DC Converter Power Management Applications

Riverside, Calif., June 17, 2014  - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new series of semi-shielded power inductors. The semi-shielded SRN model series combines the features of non-shielded and shielded inductors, making them ideal for use in DC/DC converters, which provide power management to mobile electronic devices, computers, data storage devices and consumer electronics. Bourns' SRN series is also well-suited for industrial applications such as LED lighting, control circuits and GPS equipment.

Bourns' new semi-shielded power inductor series includes models SRN2010, SRN2012, SRN2510, SRN2512, SRN4012, SRN4026, SRN5040 and SRN6028. The power inductor family delivers high inductance with an inductance range of 0.24 to 220 μH. The series also features high-rated current with Irms up to 4.7 A and Isat up to 8 A. All the models are RoHS compliant* and halogen free**.

"Bourns designed its new power inductor family using semi-magnetic shielding technology instead of the conventional ferrite shield. Preventing uncontrolled magnetic coupling of the windings, the shielding compound is applied to the perimeter of the inductor, which envelops the winding, resulting in enhanced magnetic shielding and lower radiation emissions compared to non-shielded inductors," said Guido Zehnder, product manager at Bourns, Inc. "In addition, our new power inductors have a greatly reduced footprint and are more cost-effective compared to competitively-sized conventional ferrite shield inductors."

Pricing and Availability As a pricing reference, the Bourns® model series is priced at $0.12 in 25k piece quantities, depending on model size. All models in the Bourns® SRN series are available now. For additional product specifications, please go to: www.bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

**Bourns follows the prevailing definition of "halogen free" in the industry. Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com