Search
Languages

Bourns Announces New Options to its Industry-Leading Line of Guitar Potentiometers

Riverside, Calif., January 15, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that it has released new product options to its industry-leading line of Model 95 Premium Guitar Potentiometers. Bourns developed this specialty line of potentiometers in response to customer requests for additional taper and resistance value options that help improve the sound quality, reliability and longevity in electric and bass guitars. The four new guitar potentiometer options from Bourns are being released in tandem with the upcoming NAMM Show, January 23-26, 2014 in Anaheim, California.

"Bourns continues to introduce new product options that help our customers get the highest quality out of their guitars and associated professional audio equipment," said Chuck Manzano, Pro Audio Application Engineer at Bourns, Inc. "We have an ongoing commitment to provide a variety of options for both guitar designers (luthiers) and those guitarists who customize their guitars in search of the right tone. We are thrilled to provide our customers with the highly-requested 300 ohm resistance value, which is a long-time standard value used by one of the top U.S. guitar manufacturers."

Bourns' new selection of linear tapers and resistance values allow for a slower gain on volume controls, and enable enhanced adjustability of tone controls. In addition, the superior design qualities of Bourns' long bushing potentiometers mean they are compatible for use in solid body guitars as well as in all types of electric and bass guitars. As with the complete line of Bourns Model 95 Premium Guitar potentiometers, these new options feature conductive polymer elements and multi-finger contact springs for low noise/impedance, long rotational life and dust protection for ease of maintenance, and smooth rotational operation for the discerning guitarist.

The four new configurations for the Bourns® Model 95 premium guitar potentiometer complement the variety of hand crafted parts and options already available:

Part NumberTaperShaftBushingResistance Value (kΩ)
95A1D-Z28-EA0/321LLinearKnurledStandard300
95A1D-Z28-EA0/322LLinearKnurledStandard500
95Z1D-Z33-EA0/323LLinearKnurledLong300
95Z1D-Z33-EA0/324LLinearKnurledLong500

As a pricing reference, part numbers 95A1D-Z28-EA0/321L and 95A1D-Z28-EA0/322L with standard bushing are priced at $8.03. Part numbers 95Z1D-Z33-EA0/323L and 95Z1D-Z33-EA0/324L with long bushing are priced at $12.67. All prices are based on quantities of 1,000. These new options are available through selected Bourns authorized distributors and Pro Audio resellers.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com