Search
Languages

Bourns Expands Line of Riedon™ Industrial Shunt Resistors with Six New Model Types

New models deliver superior current handling capabilities to meet accurate measurement requirements in applications ranging from renewable energy to industrial power systems

RIVERSIDE, Calif., August 26, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the expansion of its line of Riedon™ Industrial Shunt Resistors with the release of six new model types. The new shunt resistors feature superior current handling capabilities that meet accurate current measurement requirements. Precise measurements are necessary in a wide range of applications including battery management systems (BMS), solar inverters, welding equipment, heat-treating equipment, battery chargers, power supplies, cathodic protection rectifiers, and marine and mobile accessories.

The new industrial shunt resistor models are available with panel and busbar mounting options. The Riedon™ Model RSN and RS Series shunts by Bourns are panel mount products with a current handling capacity from 1 A to 1200 A, resistance values from 0.0417 milliohms to 100 milliohms and tolerances from 0.25 percent to 1 percent. The Riedon™ Model RSH, RSI, RSJ, and RSW Series shunts by Bourns are designed for direct mounting to busbars with a current capacity from 5 A to 6000 A, resistance values from 0.025 milliohms to 10 milliohms and tolerances of 0.25 percent.

All Riedon™ industrial shunt resistors by Bourns are precision shunts that incorporate low-resistance Manganin™ as their resistive material. These new shunts also offer a wide operating temperature range of -40 °C to +100 °C, and feature a compact size and center-mounted voltage taps that streamline and simplify system implementations.

All six Riedon™ industrial shunt resistor by Bourns model types are available now, and are RoHS* compliant. For additional information, please see: www.bourns.com/products/resistors/current-sense-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

In April 2023, BE Services Company, Inc., a subsidiary of Bourns, Inc., purchased certain assets of Riedon, Inc., including its logo and trademarks and the right to continue to manufacture former Riedon™ products. “Riedon Logo” is a registered trademark of BE Services Company, Inc. in the United States. “Riedon” is a trademark of BE Services Company, Inc.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com